DRV88xx Programming And Testing

1. It is recommended for the user to first install the MPROG/FTPROG EEPROM Programming Application. This tool can be downloaded from http://www.ftdichip.com/Support/Utilities.htm
2.  It is recommended for the user to first install the FET PRO430 application. These application can be downloaded from the web, or a similar MSP430 programming tool can be used.
3. After applications have been installed, follow the instructions on the DRV88xxEVM_Programming_Readme.doc file. It details how to program the USB chip serial number and the on board microcontroller firmware.
4. USB Chip and Microcontroller can be programmed in parallel.